AXIS#.FAULTED
Description
Indicates if a fault is present on the Axis. If a fault is present the value will be 1, if no faults are present, the value will be 0.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 - 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.FAULTS |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5024 |
1 |
5024 (0x13a0) |
AXIS1.FAULTED |
Unsigned8 |
Read Only |
Yes |
|
70560 |
2 |
5024 (0x13a0) |
AXIS2.FAULTED |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.FAULTED |
5024 |
Unsigned8 |
Read Only |
- |